SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
After device configuration, the bootloader performs a standard BOOTP/TFTP boot. The device sends a BOOTP request with its MAC address to a host TFTP server to be assigned an IP from a pool of addresses. After this connection is established, the device is able to receive image data encapsulated in Ethernet packets, see Section 4.6.6.2.1. Data received is stripped of its network headers and the boot data is stored in internal RAM. When the transfer completes and the image is found in good integrity, the ROM Code will branch to the address defined in the Boot Info field of the boot header.