SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
This register contains the routeid and orderid of the transaction error that was captured.
Bits | Field | Type | Reset | Description |
---|---|---|---|---|
31:28 | Reserved | r | 0x0 | Reserved. Read as 0. |
27:16 | tag | r | 0x0 | Tag – This indicates the CID/RID/SID of the transaction on the destination side of the gasket. This is the tag assigned to the transaction. For an Unexpected Transaction Error, this field is whatever the sid/rid of the transaction was.For a Timeout Error, this is the tag (replacement CID) that was used. |
15:12 | Reserved | r | 0x0 | Reserved. Read as 0. |
11:0 | cid | r | 0x0 | Command ID – This indicates the original Command ID (SID/RID) of the command. This field is only valid on a Timeout Error, not on an Unexpected Transaction Error. |