SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
Ethernet port 1
This statistic indicates the number of IEEE 802.3X pause frames transmitted by the port.
Pause frames cannot contain a CRC error because they are created in the transmitting MAC, so these error conditions have no effect upon the statistic. Pause frames sent by software will not be included in this count.
Since pause frames are only transmitted in full duplex, carrier loss and collisions have no effect upon this statistic.
Transmitted pause frames are always 64-byte multicast frames so will appear in the Tx Multicast Frames and 64octet Frames statistics.