All ports
The total number of 64-byte frames received and transmitted on the port. Such a frame is defined to be:
- Any data or MAC control frame which was destined for any unicast, broadcast or multicast address
- Did not experience late collisions, excessive collisions, or carrier sense error
- Was exactly 64 bytes long. (If the frame was being transmitted and experienced carrier loss that resulted in a frame of this size being transmitted, then the frame will be recorded in this statistic).
CRC errors, code/align errors and overruns do not affect the recording of frames in this statistic.