SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
To de-queue an entry the consumer will read the entry contents from the Proxy thread location allocated by the system, with the queue offset for the queue to access. The proxy will read the entry from the RA queue. The consumer can then read the entire contents of the entry. The completion offset (final byte of the data) will cause the proxy to flush that entry (so that it can fetch a new one from the RA upon the next read).