SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
When in idle state, the first read to the proxy will put the proxy into read state, and the proxy will read the target and channel requested in a single burst of the target's channel size. When the data is returned it is stored in the buffer and the accessed part is returned to the host. Further legal reads are allowed and return the accessed data in the buffer. When there is a legal read to the last byte of the resource, the accessed data is returned, and the proxy is put back into idle state.