SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The Egress Operation register allows enabled classifiers with any match like IPSA or IPDA match to use the CPSW Egress Packet Operations Inter VLAN Routing sub functions. If the packet was destined for the host or is destined to any port without any errors, but matches a clasifier that has a programmed egress opcode, it will be forwarded to the destination ports where the destination ports will use the thier egress opcode entry to modify the packet. InterVLAN Routing and mirroring need to be understood, they are orthogonal functions. Care must be taken not to violate VLAN rules as this can redirect packets based on classifier matches.
Return to Summary Table
| Instance Name | Physical Address |
|---|---|
| CPSW0 | 0803 E0FCh + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| EGRESS_OP | |||||||
| R/W | |||||||
| 0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| EGRESS_TRK | TTL_CHECK | RESERVED | |||||
| R/W | R/W | NONE | |||||
| 0h | 0h | 0h | |||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| NONE | |||||||
| 0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | DEST_PORTS | ||||||
| NONE | R/W | ||||||
| 0h | 0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31:24 | EGRESS_OP | R/W | 0h | The Egress Operation defines the operation performed by the CPSW Egress Packet Operations 0: NOP : 1-n: Defines which egress Operation will be performed. This allows Inter VLAN routing to be configured for high bandwidth traffic, reducing CPU load. 0xff: Swap SA and DA of packet, this is intended to allow OAM diagnostics for a link. |
| 23:21 | EGRESS_TRK | R/W | 0h | The Egress Trunk Index is the calculated trunk index from the SA, DA or VLAN if modified to that InterVLAN routing will work on trunks as well. The DA, SA and VLAN are ignored for trunk generation on InterVLAN Routing so that this field is the index generated from the Egress Op replacements elclusive or'd together into a three bit index. |
| 20 | TTL_CHECK | R/W | 0h | The TTL Check will cause any packet that fails TTL checks to not be routed to the Inter VLAN Routing sub functions. The packet will be routed to the host it was destined to. |
| 19:3 | RESERVED | NONE | 0h | Reserved |
| 2:0 | DEST_PORTS | R/W | 0h | The Destination Ports is a list of the ports the classified packet will be set to. If a destination is a Trunk, all the port bits for that trunck must be set. |