SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
This device requires several Boot Mode controls to enable device boot. The BOOTMODE inputs are not implemented on dedicated pins. They are multiplexed with other signal functions, where pins associated with the BOOTMODE inputs are defined in the Pin Attributes table. The logic state of the BOOTMODE inputs are latched on the rising edge of PORz_OUT. Valid logic states must be maintain as long as PORz_OUT is held low. The latched values are reflected in WKUP CTRL MMRs for read/write access.