SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The AASRC channel is controlled primarily via the channel's TxFifoConfig register. This register holds 3 basic pieces of information:
The channel remains idle until a pulse is detected on ALL associated input DMA request event pins required by the TxFifoConfig setting. The pulses for the individual events are latched and held by the PDMA until they all arrive.
Once the channel activates, it starts reading FIFO index values from the TxOrderTable, starting at the configured 'First Slot' and ending with the 'Last Slot'. The actual FIFO indices used are obtained from the ordering table. For example, say FirstSlot=3 and LastSlot=5. If the first 6 slots of the ordering table were: 0, 2, 4, 6, 8, 10, the FIFOs written for the event would be 6, 8, and 10, because 'slot 3' of the table contains 6, and it would proceed through 'slot 5' of the table which contains 10.
The X and Y registers are still used as they are in a normal X-Y mode. When accessing each FIFO, the setting of X determines the sample byte width written to the FIFO. The value of 'Y' determines how many times the entire FIFO list is processed for each activation of the channel.
Once the total specified number of transactions has been completed, the channel returns to an idle state and waits until it is triggered again. The write transfers that are performed are accomplished as quickly as possible, given availability of data in the TX channelized FIFO and given the arbitration that may occur as a result of other channels also using the same write unit.