SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
In reception, there are 2 ways to stop it
There is a limitation when receiving data in UART CIR mode. The IrDA transceivers on the market have a common characteristic that shrinks the hold time of the received modulation pulse. The UART filtering schema on receiving is based on the same encoding mechanism used in transmission.
For the following scenario:
So the data sent in those conditions would look like 7us pulses within 28us period. The UART expects to receive similar incoming data on receive, but available transceiver timing characteristics typically send 2us modulated pulses. Those will be filtered out and RX FIFO will not receive any data.
This does not affect UART CIR mode in transmission.
The CIR RX demodulation can be bypassed by setting the UART_MDR3[0] DISABLE_CIR_RX_DEMOD bit.