SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The transmit high-speed and transmit clock configuration is controlled by the following registers:
In case, the transmit bit clock, ACLKX, is generated internally, the MCASP_ACLKXCTL[5] CLKXM bit must be set to 1. Thus, the clock is divided down by a programmable bit clock divider (the MCASP_ACLKXCTL[4-0] CLKXDIV bit field) from the source signal.
If the transmit high-frequency controller clock, AHCLKX, is also sourced internally (that is first scenario described in Section 12.1.2.4.2, the MCASP_AHCLKXCTL[15] HCLKXM bit must be set to 1. Thus, the clock is divided down by a programmable high-clock divider (the MCASP_AHCLKXCTL[11-0] HCLKXDIV bit field) from the MCASP internal clock source AUXCLK.
Internally, the MCASP always shifts transmit data at the rising edge of the internal transmit clock - XCLK, (see Figure 12-21). The CLKXP mux determines if ACLKX needs to be inverted to become XCLK. If MCASP_ACLKXCTL[7] CLKXP = 0, the CLKXP mux directly passes ACLKX signal to XCLK. As a result, the MCASP shifts transmit data at the rising edge of ACLKX. If MCASP_ACLKXCTL[7] CLKXP = 1, the CLKX mux passes the inverted version of ACLKX to XCLK. As a result, the MCASP shifts transmit data at the falling edge of ACLKX.
It can be seen in Figure 12-21 that XCLK is propagated to the Rx clock logic, to allow an internally synchronous operation between MCASP transmitters and receivers. This is used for example in the MCASP loopback mode.
The polarity of ACLKX can be controlled in the MCASP_ACLKXCTL[7] CLKXP bit, regardless of ACLKX signal being internally or externally sourced.
In addition, there is an option to invert polarity of the AHCLKX controller high speed clock via writing the MCASP_AHCLKXCTL[14] HCLKXP bit.
In a similar way, the polarity of AHCLKX clock can be controlled in the MCASP_AHCLKXCTL[14] HCLKXP bit, regardless of the AHCLKX signal being internally or externally sourced.
Figure 12-21 presents the block diagram of the transmit clock generator.
Figure 12-21 Transmit Clock Generator Block DiagramIn this device:
For more information about MCASP integration, see Section 12.1.2.2, MCASP Environment, and Module Integration.