SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The intent of the Data Movement architecture is to provide a uniform HW/SW interface which includes a rich set of mechanisms that SW can make use of to transfer data with low overhead and reasonable complexity. To this goal, the number of components which SW is required to interact with on an ongoing real time basis has been kept to a minimum and is as follows (in order of anticipated frequency of access):
Interrupt Aggregator
Packet DMA
Block Copy DMA
When interrupts are used, the interrupt aggregator will provide the vast majority of interrupt sources from all DMA components in the system. Each non-exception/non-debug packet and TR completion signaling originates from the Interrupt Aggregator and the IA provides a uniform set of MMRs that can be queried to quickly determine the cause of a specific interrupt. Events from PSI-L/ETL components are all routed to the host via the Interrupt Aggregator.
Each PKTDMA and BCDMA instance includes an inbuilt ring control mechanism which is the primary means by which work is sent to or received from these DMAs. Each DMA instance also includes both static configuration type memory mapped registers and some real-time accessible memory mapped registers for monitoring and control of each individual channel.
Memory mapped data structures are used anytime information needs to be passed between components in the system. These components may be hardware or software. The following sections describe the data structures which are used within the DMSS for passing information. These data structures include data buffers, packet descriptors, buffer descriptors, queues (including transmit queues, transmit completion queues, and receive queues) and the configuration MMRs that are provided in the various components. The following sections provide a detailed description of these data structures.