SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The next diagram expands the 32-bit FLAGS field. The numbers above each field here indicate bit numbers within the field.
31 | 24 | 23 | 16 | |||||||||||||||
CONFIGURATION SPECIFIC FLAGS | Reserved | |||||||||||||||||
15 | 8 | 7 | 5 | 4 | 3 | 0 | ||||||||||||
TRIGGER_SIZE1 | TRIGGER1 | TRIGGER_SIZE0 | TRIGGER0 | EVENT_SIZE | WAIT | STATIC | TYPE | |||||||||||
The flags field fills in the remaining details about the stream, as follows:
Bit | Field | Description |
|---|---|---|
0-3 | TYPE | The TYPE of TR that is being sent 0: One dimensional data move 1: Two dimensional data move 2: Three dimensional data move 3: Four dimensional data move 4: Four dimensional data move with data formatting 5: Four dimensional Cache Warm 6-7: Reserved 8: Four Dimensional Block Move 9: Four Dimensional Block Move with Repacking 10: Two Dimensional Block Move 11: Two Dimensional Block Move with Repacking 12-14: Reserved 15 Four Dimensional Block Move with Repacking and Indirection |
4 | Reserved | Reserved for Future use. |
5 | WAIT | This field is only valid on Type 15 TRs. This field indicates whether or not this TR should ensure it completes before allowing the next TR to start on this channel. The encoding is as follows: 0 = Allow next TR to start immediately 1 = Wait for this TR to complete before allowing next TR to start When set, the next TR will not be considered triggered (regardless of any other trigger conditions) until all write status responses for the current TR have landed. |
6-7 | EVENT_SIZE | This is how often the TR will generate an output event. 0: Event is only generated with the TR is complete 1: Event is generated when the second inner most loop (ICNT1) is decremented by 1. 2: Event is generated when the third inner most loop (ICNT2) is decremented by 1. 3: Event is generated when the outer most loop (ICNT3) is decremented by 1. |
8-9 | TRIGGER0 | This is one of two selectable triggers. The receipt of this trigger will enable the TR to be active for enough data transfer as specified by the TRIGGER0_TYPE Field. 0: No Trigger 1: Global Trigger 0 for the channel 2: Global Trigger 1 for the channel 3: Local Event for the channel |
10-11 | TRIGGER0_TYPE | This is the type of data transfer that will be enabled by receiving a trigger. 0: The second inner most loop (ICNT1) will be decremented by 1. 1: The third inner most loop (ICNT2) will be decremented by 1. 2: The outer most loop (ICNT3) will be decremented by 1. 3: The entire TR will be allowed to complete. |
12-13 | TRIGGER1 | This is one of two selectable triggers. The receipt of this trigger will enable the TR to be active for enough data transfer as specified by the TRIGGER1_TYPE Field. 0: No Trigger 1: Global Trigger 0 for the channel 2: Global Trigger 1 for the channel 3: Local Event for the channel This field is reserved for a Direct TR. |
14-15 | TRIGGER1_TYPE | This is the type of data transfer that will be enabled by receiving a trigger. 0: The second inner most loop (ICNT1) will be decremented by 1. 1: The third inner most loop (ICNT2) will be decremented by 1. 2: The outer most loop (ICNT3) will be decremented by 1. 3: The entire TR will be allowed to complete. |
16-23 | Reserved | Reserved for Future use. |
24-31 | Configuration Specific Flags | These are flag bits that can be specified by the specific BCDMA configuration. These bits will remain undefined in the global TR format to allow for customization requirements that might be required in the specific BCDMA implementation. |