SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
This register selects which channel make up the Output group 0. This is used for group event generation and group mode settings.
Return to Summary Table
| Instance Name | Physical Address |
|---|---|
| AASRC0 | 02D0 0094h |
| AASRC1 | 02D4 0094h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R | |||||||
| 0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R | |||||||
| 0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| CHANNEL_15_GROUP_ENABLE | CHANNEL_14_GROUP_ENABLE | CHANNEL_13_GROUP_ENABLE | CHANNEL_12_GROUP_ENABLE | CHANNEL_11_GROUP_ENABLE | CHANNEL_10_GROUP_ENABLE | CHANNEL_9_GROUP_ENABLE | CHANNEL_8_GROUP_ENABLE |
| R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
| 0h | 0h | 0h | 0h | 0h | 0h | 0h | 0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| CHANNEL_7_GROUP_ENABLE | CHANNEL_6_GROUP_ENABLE | CHANNEL_5_GROUP_ENABLE | CHANNEL_4_GROUP_ENABLE | CHANNEL_3_GROUP_ENABLE | CHANNEL_2_GROUP_ENABLE | CHANNEL_1_GROUP_ENABLE | CHANNEL_0_GROUP_ENABLE |
| R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
| 0h | 0h | 0h | 0h | 0h | 0h | 0h | 0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31:16 | RESERVED | R | 0h | Always read as 0 |
| 15 | CHANNEL_15_GROUP_ENABLE | R/W | 0h | Output Channel 15 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 14 | CHANNEL_14_GROUP_ENABLE | R/W | 0h | Output Channel 14 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 13 | CHANNEL_13_GROUP_ENABLE | R/W | 0h | Output Channel 13 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 12 | CHANNEL_12_GROUP_ENABLE | R/W | 0h | Output Channel 12 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 11 | CHANNEL_11_GROUP_ENABLE | R/W | 0h | Output Channel 11 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 10 | CHANNEL_10_GROUP_ENABLE | R/W | 0h | Output Channel 10 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 9 | CHANNEL_9_GROUP_ENABLE | R/W | 0h | Output Channel 9 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 8 | CHANNEL_8_GROUP_ENABLE | R/W | 0h | Output Channel 8 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 7 | CHANNEL_7_GROUP_ENABLE | R/W | 0h | Output Channel 7 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 6 | CHANNEL_6_GROUP_ENABLE | R/W | 0h | Output Channel 6 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 5 | CHANNEL_5_GROUP_ENABLE | R/W | 0h | Output Channel 5 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 4 | CHANNEL_4_GROUP_ENABLE | R/W | 0h | Output Channel 4 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 3 | CHANNEL_3_GROUP_ENABLE | R/W | 0h | Output Channel 3 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 2 | CHANNEL_2_GROUP_ENABLE | R/W | 0h | Output Channel 2 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 1 | CHANNEL_1_GROUP_ENABLE | R/W | 0h | Output Channel 1 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |
| 0 | CHANNEL_0_GROUP_ENABLE | R/W | 0h | Output Channel 0 Group Enable indicates if the Output Channel is part of the group0 for the group settings and interrupt event generation If this bit is set then the group event and interrupt will not fire until the threshold condition for this Output Channel is met. Writing 1 will enable and Writing 0 will disable 0 This channel is not part of this group 1 This channel is part of this group |