SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
The basic purpose for the RTC is to keep time of day. The other equally important purpose of RTC is for Digital Rights management. Some degree of tamper proofing is needed to ensure that simply stopping, resetting, or corrupting the RTC does not go unnoticed so that if this occurs, the application can re-acquire the time of day from a trusted source. The final purpose of the RTC is to wake the rest of chip up from a power down state.