SPRUJC6A December 2024 – July 2025 AM2752-Q1 , AM2754-Q1
This mode is used if the DMTIMER1MS_TSICR[2] POSTED bit is set to 1 (default value).
This mode uses a posted write scheme to update any internal register (DMTIMER1MS_TCLR, DMTIMER1MS_TCRR, DMTIMER1MS_TLDR, DMTIMER1MS_TTGR, DMTIMER1MS_TMAR, DMTIMER1MS_TPIR, DMTIMER1MS_TNIR, DMTIMER1MS_TCVR, DMTIMER1MS_TOCR, and DMTIMER1MS_TOWR). Therefore, the write transaction is immediately acknowledged on the configuration interface, although the effective write operation occurs later because of a resynchronization in the timer clock domain. The advantage is that neither the interconnect, nor the device that requested the write transaction is stalled.
For each register, a status bit is provided in the timer write-posted status (DMTIMER1MS_TWPS) register. In this mode, it is mandatory that software check this status bit before any write access. If a write is attempted to a register with a previous access pending, the previous access is discarded without notice.
The timer module updates the value of the timer counter register synchronously with the interface clock. Consequently, any read access to DMTIMER1MS_TCRR does not add any resynchronization latency; the current value is always available.
Because the overflow IRQ is generated when the value of DMTIMER1MS_TCRR reaches 0xFFFF FFFF, and not when it changes its value to the value after overflow, it is necessary to wait a delay of (1 × PS × timer functional clock period) before any read access to DMTIMER1MS_TCRR to ensure a correct reading of its content.
If DMTIMER1MS_TTGR register is written during a posted write to DMTIMER1MS_TCRR, the value to be written to DMTIMER1MS_TCRR will be discarded.
If a posted write to DMTIMER1MS_TCVR is started, the user must not write to DMTIMER1MS_TPIR or DMTIMER1MS_TNIR before the DMTIMER1MS_TCVR write is finished, because the value of DMTIMER1MS_TCVR is re-evaluated, so both the value to be written, and the recalculated value will be discarded.
If a write access is pending for a register, reading from this register does not yield a correct result. Software synchronization must be used to avoid incorrect results.
Functional frequency range: freq(timer clock) < freq(interface clock)/4.